web
You’re offline. This is a read only version of the page.
close
Support Portal

SICK Nova 2.10.0 release

Release notes for the SICK Nova 2.10.0 release.
Related Products
Ruler3010
Visionary-T Mini AP
InspectorP63x
Ruler3060
Ruler3002
InspectorP61x
Inspector85x
InspectorP64x/InspectorP65x
Ruler3004
Ruler3008
Ruler3020
Ruler3120
SICK Nova
InspectorP62x
Inspector83x
edge computing devices

Table of Contents

Highlights of the 2.10.0 release

AI Object Detection tool

Among the many new features we are extra thrilled to present a new AI-powered tool for the Inspector8xx-series; the AI Object Detection tool. 

 

  • AI Object Detection supports on-device training and is suitable for finding features within objects in acquired images. The tool is trained using up to 100 images and is ideal for counting applications. The result is visualized as a point on the detected object.
  • AI Object Detection (dStudio) supports training using the SICK dStudio service and is used to detect (i.e. find) objects in acquired images. The resulting objects are found as bounding boxes which are characterized by their class, size and position.
Nova Dashboard

Another big news is the configurable Dashboard for Nova. The dashboard is easily configured with widgets for e.g. showing sensor data and results in an clean-looking overview.

 

Tool menu with categories

For even easier navigation, the analysis tools have now been sorted into categories in the tool menu.

 

Nova 2D analysis tools for Nova 3D

And that's not all, the 2.10 release also brings a number of Nova 2D analysis tools to Nova 3D, including 1D/2D Code DPM for Nova Ruler3000 and color tools for Visionary-S.

 

Blob Verifier tool for Nova Ruler3000

Talking about new tools for Nova Ruler3000, the 2.10 version adds the Blob Verifier tool, which checks that the found blobs in the image match with a taught set of blobs.

 

Machine Vision Viewer 1.0.0

Besides the update for SICK Nova, we also release a completely new software; Machine Vision Viewer 1.0.0. The software enable easy viewing of saved sensor images, in both 2D and 3D and supports a wide range of formats, including MV3. Download it here.

 

Nova recording tool 1.2.0

We The device scanning is now significantly faster when scanning on a network with several devices connected. Download it here.

 

Machine Vision ZIP .NET SDK 1.1.0

There is an official SDK for .NET to both simplify integration for other SICK products and for customers using the MVZ formatMachineVisionZip SDK for .NET 1.1.0. Download it here.

 

Nova 2D

Nova Inspector

The main news for Nova Inspector 2.10.0 (incl. Quality Inspection and Intelligent Inspection) compared to Inspector v2.9.0:

  • New tools: AI Object Detection and AI Object Detection (dStudio) (Available for Inspector8xx-series)
  • New tool: Noise Reduction Filter
  • New tool: Morphology Filter
  • Tool menu with categories
  • Configurable dashboard for operator UI
  • AI tool improvements

Nova picomidiCam2 

The main news for Nova picomidiCam2 2.10.0 (incl. Quality Inspection and Intelligent Inspection) compared to Nova SIM 2D v2.9.0:

  • Package renamed to Nova picomidiCam2
  • New tool: Noise Reduction Filter
  • New tool: Morphology Filter
  • Tool menu with categories
  • Configurable dashboard for operator UI
  • AI tool improvements
 

Nova 3D

Nova Ruler3000

The main news for Nova Ruler3000 v2.10.0 (incl. Quality Inspection) compared to Nova SIM 3D v2.9.0:

  • Package renamed to Nova Ruler3000
  • New tools: 2D analysis tools in Nova 3D
  • New tools: 1D/2D Code DPM
  • New tool: Blob Verifier
  • New tool: Morphology Filter
  • Tool menu with categories

Nova Ruler3000 IPC

There is now an IPC solution for SICK Nova to run with Ruler3000. With the specific Nova Ruler3000 IPC SensorApp running on SICK AppEngine, the Ruler3000 enable high performance quality control applications to be solved in unmatched speed.

  • Sensor Connection
    The tool Sensor Connection scans for and connects to a Ruler3000 camera.

  • Acquisition settings for Ruler3000
    The Acquisition section contains settings for the Ruler3000 camera, such as configuring the laser detection, image trigger, motion, and field of view.

  • Configurable dashboard for operator UI
    A configurable dashboard with widgets for e.g. showing sensor data and results has been added.

  • Many 2D and 3D analysis tools
    See full release notes for details.

Nova Visionary-S

The main news for Nova Visionary-S 2.10.0 (incl. Presence Inspection and Quality Inspection) compared to Nova Visionary-S v2.9.0:

  • New tools: 2D analysis tools in Nova 3D
  • New tool: Blob Verifier
  • New tools: Color tools
  • New tool: Color Classification
  • New tool: Probe Color

Nova Visionary-T Mini

The main news for Nova Visionary-T Mini 2.10.0 (incl. Presence Inspection and Quality Inspection) compared to Nova Visionary-T Mini 2.9.0:

  • New tools: 2D analysis tools in Nova 3D
  • New tool: Blob Verifier
  • New tool: Morphology Filter
  • Tool menu with categories
  • Configurable dashboard for operator UI

Nova LMS4000

The main news for Nova LMS4000 2.10.0 (incl. Presence Inspection and Quality Inspection) compared to Nova LMS4000 2.9.0:

  • New tools: 2D analysis tools in Nova 3D
  • New tool: Blob Verifier
  • New tool: Morphology Filter
  • Support for additional LMS variants
  • Configurable input logic for external trigger
Keywords:
Nova, SICK Nova, Quality Inspection, Intelligent Inspection, Nova API, SICK Nova API, Nova Recording Tool, Nova Recording Tool Download, Nova release notes