web
You’re offline. This is a read only version of the page.
close
Support Portal

What screws are needed to mount solid shaft encoders with a square flange?

Table of Contents

4xM5 Hexagon socket head cap screws e.g. DIN EN ISO 4762 should be used to mount rotary encoders with a square flange.

In addition, please also use some M5 washers e.g. DIN EN ISO 7092 for these screws.

The screw length depends on the application.

Keywords:
rotary encoders, solid shaft encoders, square flange, mounting, screws, washers