motion control sensors
absolute encoders - Latest Knowledge Articles
Application
(Show all)Mounting Rotary Encoders- Guidelines, Information & Mounting Videos
Mounting Rotary Encoders- Guidelines, Information & Mounting Videos
How to mount an encoder with face mount flange onto an EG34x safety limit switch?
How to mount an encoder with face mount flange onto an EG34x safety limit switch?
FAQ
(Show all)What screws are usually used to mount the stator coupling to the hollow shaft encoders?
What screws are usually used to mount the stator coupling to the hollow shaft encoders?
Which servo clamps can be used for which encoder? In which pitch circle diameter do the servo clamps have to be mounted?
What encoder groups are there for encoders with a servo flange regarding the centering and the servo groove width/diameter?
Tutorial
(Show all)How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?
How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?