web
You’re offline. This is a read only version of the page.
close
Support Portal

TiM - HDDM vs HDDM+ in foggy environments

Describes how to measure different types of meteorology in fog conditions.
Related Products
TiM-S
TiM3xx
TiM5xx
TiM7xx

Table of Contents

The different TiM variants are using slightly different technologies (see related article).

This results in different measurement behavior under certain conditions.
In a foggy environment, TiMs with hddm technology are less sensitive than HDDM+ devices.


In the following screenshots, you can see the scan view of two TiMs with the wo different technology (HDDM & HDDM+) in foggy environments (visibility ~220 Meteorological Optical Range - MOR).

HDDM+




HDDM



Test:
The two test devices (TiM771-S and TiM781-S) are looking in the same direction and have the same configured fields (field 1= 1m*1m, field 2=2m*1m). The recording tool counts every field detection and combines it with the environment visibility.

Results:



The TiM781(HDDM+) fields are active when the visibility falls under 230. The TiM771(HDDM) shows no reaction.

 

Keywords:
TiM3xx, TiM5xx, TiM7xx, fog, HDDM, HDDM+