web
You’re offline. This is a read only version of the page.
close
Support Portal

CANopen EDS-Files for 4Dpro devices

Overview of available EDS files and CANopen guides

Table of Contents

CANopen EDS-files 4Dpro

Supported interfaces: CANopen in 4Dpro devices on board

To use CANopen with the 4Dpro devices the below EDS Files can be used.
See this Manual_CANopen_SICK-Ident_V17.pdf for general handling. The Manual is already included in the EDS ZIP file.

 

When you use CAN-Open you loose the option to run Master/Slave or Multiplexer/Server. As well it is at CAN-Open not possible to program with SOPAS via CAN. These Options are only given at Sick CAN Scanner Network.

 

 You can use CAN-Open or SICK CAN Scanner Network, but not both at same time. Use only devices with build in CAN-Interface.  

Device CANopen EDS and Manual SICK CAN Scanner Network

Lector61x-62x

SICK_Lector61x-62x_CANopen_package.zip Master/Slave, Multiplexer/Server, SOPAS Hub
Lector63x SICK_Lector63x_CANopen_package.zip Master/Slave, Multiplexer/Server, SOPAS Hub
Lector64x-65x --- Master/Slave, Multiplexer/Server, SOPAS Hub
CLV61x --- Master/Slave, Multiplexer/Server, SOPAS Hub
CLV62x-65x SICK_CLV62x-65x_CANopen_package.zip Master/Slave, Multiplexer/Server, SOPAS Hub
CLV69x --- Master/Slave, Multiplexer/Server, SOPAS Hub
RFH62x-63x SICK_RFH6x_CANopen_package.zip Master/Slave, Multiplexer/Server, SOPAS Hub
RFU61x --- ---
RFU62x-65x SICK_RFU62x-65x_CANopen_package.zip Master/Slave, Multiplexer/Server, SOPAS Hub

--- not implemented

CANopen Example using proCANtool

Here an CAN-Open PC-Adapter from EMS Wuensche is used to demontstrate the commuication: CANopen_Example_using_PC-Adapter.pdf

CANopen Example using CANopen DeviceExplorer

SICK CAN Scanner Network (CSN) features

  • Master/Slave: Can be used to get only one (common) result from a group of devices.
  • Multiplexer/Server: Here each device is individual triggered and each result is passed to the host including the address of the server.
  • With SOPAS HUB Addressing each device can be parameterized using SOPAS via the CAN-Bus. Viewing or transfer of picture is not possible.
Keywords:
canopen, EDS, eds file, 4dpro, rfu6xx, rfh6xx, clv, lector6, can bus, Sick Can