web
You’re offline. This is a read only version of the page.
close
Support Portal

What is the mounting spigot and how does it work?

Table of Contents

The mounting spigot has a centering recess for the respective encoder, which is slotted towards the top.

There is a threaded hole on one side of the slot and a flat countersink for a cylinder head screw on the other.

 

Tightening the screw causes the slots to contract, clamping the encoder in place. The production of the mounting spigot is somewhat more complex, but no additional screws are required, and installation is straightforward.

 

As the mounting spigot is also a centering fixture, it must be designed to prevent angles or shaft offset during clamping.

Keywords:
rotary encoders, solid shaft encoders, face mount flange, mounting spigot