web
You’re offline. This is a read only version of the page.
close
Support Portal

Why is the CFS50 on SICK.com in the Archive? Is it phased out?

What is the current status of the CFS50

Table of Contents

What is the CFS50?

The CFS50 is an incremental motor feedback system with commutation signals (block commutation). This encoder series is used servo motor applications (inside the motor).
The previous encoder series was the CNS50 (see the linked Knowledge Article KN-09858).

 

For more detailed information, please check the attached data sheet:

The CNS50 is using the F-technology

Why is the CFS50 in the Archive?

The CFS50 is not phased out. It will be still produced and customer can order it.

But we do not want to generate new business or customers with this encoder, because we do not want to keep it very long alive.

Therefore, it is no more visible at SICK.com.

 

But there is no official phase out planed so far.

Keywords:
motor feedback, motion control, drives and controls, incremental, commutation, phase out