Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
To utilize a UHF transponder, it is necessary to understand its memory structure. The structure is defined by the ISO/IEC 18000-63 standard and by the EPCglobal of GS1, so compatible readers conforming to the same standard would be able to access the memory content.
Please note that this document explains the main memory structure of UHF transponders. Depending on the transponder, there may be differences and special features that are not covered here. Further details can be found in the data sheet of the respective transponder.
UHF Memory Structure
The following picture shows a schematic structure of an UHF transponder according to ISO/IEC 18000-63 and EPCglobal.
Explanation of the different memory areas
An UHF transponder provides four different memory banks that are described below.
Reserved Memory Bank
The reserved memory bank contains the kill and access passwords. These passwords can be set manually and can be locked to prevent unauthorized changes. For more details on the kill and locking process, see thisKnowledge Article.
The kill password is 4 bytes long and is used to permanently destroy transponders. The default kill password is 0x00000000. To use the kill command, you need to set a password other than the default.
The access password has the same size of 4 bytes. It is used to restrict the access to the transponder data. The default access password is 0x00000000 as well.
UII Memory Bank
The UII (Unique Item Identifier) memory bank consists of various parts. These are explained in the following.
CRC (Cyclic Redundancy Check)
The CRC is a checksum that is calculated from the content of the PC word and UII. This is used to check if the transfered data is correct.
PC (Protocol Control)
The PC word contains information of the format of the UII/EPC. The first five MSBits (Most Significant Bits) indicate the Length of the UII/EPC.
EPC Length Indicates the length of UII/EPC in words
UMI (User Memory Indicator) Indicates whether a User Memory is active
XI (XPC_W1 Indicator) Indicates whether a XPC (Extended Protocol Control) is active
NSI (Numbering System Identifier)
If the transponder memory follows the EPCglobal structure (T=0) Bit 18h to 1Fh is used for AFI (Application Family Identifier) as defined in EPCglobal Data Standards
If the transponder memory follows the ISO structure (T=1) Bit 18h to 1Fh is Reserved for Future Use (RFU) as defined in ISO/IEC 15961
List of common used PC words and corresponding EPC Length
PC word
EPC Length
hex
bin
bits
bytes
words
0C00
0000 1100 0000 0000
16
2
1
1400
0001 0100 0000 0000
32
4
2
1C00
0001 1100 0000 0000
48
6
3
2400
0010 0100 0000 0000
64
8
4
2C00
0010 1100 0000 0000
80
10
5
3400
0011 0100 0000 0000
96
12
6
3C00
0011 1100 0000 0000
112
14
7
4400
0100 0100 0000 0000
128
16
8
4C00
0100 1100 0000 0000
144
18
9
5400
0101 0100 0000 0000
160
20
10
5C00
0101 1100 0000 0000
176
22
11
6400
0110 0100 0000 0000
192
24
12
6C00
0110 1100 0000 0000
208
26
13
7400
0111 0100 0000 0000
224
28
14
7C00
0111 1100 0000 0000
240
30
15
8400
1000 0100 0000 0000
256
32
16
8C00
1000 1100 0000 0000
272
34
17
9400
1001 0100 0000 0000
288
36
18
9C00
1001 1100 0000 0000
304
38
19
A400
1010 0100 0000 0000
320
40
20
AC00
1010 1100 0000 0000
336
42
21
B400
1011 0100 0000 0000
352
44
22
BC00
1011 1100 0000 0000
368
46
23
C400
1100 0100 0000 0000
384
48
24
CC00
1100 1100 0000 0000
400
50
25
D400
1101 0100 0000 0000
416
52
26
DC00
1101 1100 0000 0000
432
54
27
E400
1110 0100 0000 0000
448
56
28
EC00
1110 1100 0000 0000
464
58
29
F400
1111 0100 0000 0000
480
60
30
FC00
1111 1100 0000 0000
496
62
31
UII/EPC
UII (Unique Item Identifier):
The Unique Item Identifier (UII) is a term used when the transponder memory adheres to the ISO structure. In this context, the UII represents the specific identifier data stored in the RFID tag, besides the CRC (Cyclic Redundancy Check) and PC (Protocol Control) word. The UII is often used to give a transponder a unique name so it can be identified distinctly, which is crucial for inventory management, asset tracking, and other identification applications.
EPC (Electronic Product Code):
The Electronic Product Code (EPC) is used when the transponder memory follows the EPCglobal Data Standard, which is a widely adopted framework in the RFID industry. The EPC serves a similar purpose to the UII, providing a unique identifier for each item. It is stored in the RFID tag's memory along with the CRC and PC word. The EPC is designed to be a globally unique identifier, enabling seamless tracking and identification of products across different systems and organizations.
EPCglobal is a global standard that defines standardised formats and protocols, so transponders from different manufacturers and systems can be understood. Depending on the used coding scheme RFID reader can generate the Unique Ressource Identifier (URI) This enables seamless communication and interoperability in RFID applications. See the EPCglobal Data Standards for further information.
Key Differences:
Terminology: The term UII is used in the context of ISO-compliant tags, whereas EPC is used for tags that follow the EPCglobal standard.
Purpose: Both UII and EPC serve the same fundamental purpose of uniquely identifying items, but they do so within the frameworks of their respective standards.
XPC (Extended Protocol Control)
XPC (Extended Protocol Control) words are optional. They provide additional protocol control information that extends the capabilities of the basic PC word in UHF RFID tags. The XPC words are used to manage specific features and functionalities of the RFID tag. See EPCglobal Data Standards or ISO/IEC 18000-63 for further information
TID Memory Bank
The TID (Tag Identifier) memory bank is a special part of an RFID tag’s memory that holds a unique code given by the manufacturer. This code is permanent and cannot be changed.
The first Byte (MSB) of the TID contains the UHF Header E2h according to ISO 18000-6. The following three byte are indicating the tag manufacturer and the tag model. The remaining data is a worldwide unique serial number of the transponder.
User Memory Bank
The User memory bank is used to store additional information chosen by the user. This can include details like product information, process data, or any custom data. It is flexible and writable, allowing users to update the information as needed. The size of the User Memory depends on the used transponder.
Reference to SOPAS ET
The UHF transponder data can be accessed via the "Transponder Access" page in SOPAS ET or via commands. The following picture shows an example of an accessed transponder in SOPAS ET with a RFU6xx device.
Keywords: UHF, Transponder, Memory, memory structure, UII, UMEM, TID, EPC, XPC, user memory, usermem, memory bank, RFU6, EPCglobal, GS1