web
You’re offline. This is a read only version of the page.
close
Support Portal

Which mDNS hostnames are available in addition to "sec200-sick.local"?

How to easily identify and connect to a specific SEC200 without knowing its IP address.

Table of Contents

Using mDNS Hostnames to Access the SEC200

The SEC200 can be accessed using different mDNS hostnames, depending on the number of devices connected to the local network and whether a specific device needs to be addressed.


Using an mDNS hostname provides several advantages:

  • The current IP address of the SEC200 does not need to be known.
  • The hostname remains usable if the IP address changes, for example when DHCP or Auto IP is used.
  • A specific SEC200 can be identified and accessed by its serial number.
  • The hostname can be used in applications that accept a hostname or IP address.

The available mDNS hostnames depend on the number of SEC200 devices connected to the local network:


The mDNS hostname can be used, for example, to:

  • Open the SEC200 user interface in a web browser.
  • Ping the SEC200 from a terminal or command prompt.
  • Establish a TCP/IP connection using tools such as Hercules.

Network limitation

mDNS communication is limited to the local network segment because mDNS multicast traffic is normally not forwarded by routers. The computer and the SEC200 must therefore be connected to the same Layer 2 network or broadcast domain.

An mDNS hostname cannot normally be used to access an SEC200 located in another subnet, VLAN, or routed network. Cross-network resolution is only possible if the network infrastructure provides a specifically configured mDNS gateway, reflector, or repeater.

Keywords:
mDNS, hostname, webserver, connectivity