network and connection technology
Application
(Show all)IO-Link devices with high current consumption (>200mA)
The article lists some common IO-Link masters and their maximum current per port and what to do if the master doesn't deliver enough current.
Detect over height and alignment of a box with SIG100
The article explains how to detect the over height and alignment of a box with SIG100.
Speed measurement without PLC (A72 or SIG100)
The article demonstrates how to measure speed with a SIG100 or a smart sensor ...A72.
FAQ
(Show all)Are PVC cables free of halogen?
Description