detection sensors
Application
(Show all)Navigation Tree of the CSS High Speed
Here is the menu structure for configuring the CSS color sensor in the "high-speed" version with 7-segment display.
KTS versus CSS for mark detection in print applications
Pointing out why the CSS is less suitable for registration mark detection in the printing industry.
Output and CMV behavior when two or more colors are assigned to one output
Output logic of the CSS/CSX color sensor, when two or more colors are assigned to one output.