Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Important Notice: AI‑Assist 1.4.0 is incompatible with firmware 4.3.3. Firmware downgrades are not supported, so reverting to version 1.4.0 is not possible after updating.
⚙️ Software and system requirements for software installation
SICK AppManager software tool
Operating systems:
Windows 7 (32 bit and 64 bit), Windows 10 or Windows 11
Ubuntu Linux 14.04, 16.04, 18.04, 22.04 on x86_64 (64 bit)
Raspian Buster on ARM32 (32 bit)
1 GHz CPU or comparable and at least 1 GB RAM
Free hard disk space: 250 MB
Ethernet: 100 MBit/s or higher. 1 Gbit/s or faster is recommended for best performance during configuration of the device
🛠️ Installation
Please follow the instructions below and carefully read the release notes before starting the installation of the AI-Assist software.
Important Notice: Please make sure the minimum required firmware is installed. It can be found in the chapter “Supported Firmware”.
If necessary, update the device firmware before the update of the software.
🔧 Preparation: Configuration backups
The AI-Assist configuration is not preserved during the software update process. Use SICK AppManager to create a backup of the existing AI-Assist configuration. The resulting *.sbpk file can also be used to duplicate the configuration. Any licenses will be retained during the software update process.
Note: Due to major technical changes, configurations exported with AI-Assist version 1.4.0 are not fully compatible with version 2.0.2. We recommend setting up a new configuration with version 2.0.2, subsequently creating a backup of the configuration, which can then be used for duplication in future deployments.
🔄 Installing and Updating Software via Sick AppManager
To update the software of your device using Sick AppManager, follow these steps:
Launch Sick AppManager and ensure your device is connected.
In the upper left pane, click Search devices.
Double-click the listed device you want to update.
The device and app data will now appear in the lower left pane.
If the device information does not appear there, ensure that the IP configuration of your Ethernet adapter is compatible with the device IP.
In case there are any Apps installed on the device: Delete all Apps
In the upper right window pane, click on the "Local Packages" tab and choose the software file (*.sapk). If the correct software file is not listed click on the ➕ symbol (Add packages to repository).
Finally, click on install and follow the on-screen instructions.
When prompted for credentials, log in using the Service user level. User: Service Password: [your custom password] 💡 If the password has not been changed, the default is: CUST_SERV
If you have installed the AI-Assist software on a device for the first time, you must activate the software with a corresponding license key. You can obtain it on sick.com or via your local sales representative.
Updated neural network for improved person detection accuracy
Enhanced RGB image quality to improve detection, e.g. in shadowed scenes
Introduction of detection and holding time for configurable detection stability
Infringement threshold to configure minimum portion of person in a field
2D Video Livestream Overlays
Adds visualization of detected persons and objects, distance information and warning level information to livestream
2D Video Livestream Configuration
Allow enabling or disabling specific overlays (e.g. distance) in the livestream
Configurable warning level assignment for each field
Object List
Provides a list of detected classified objects including identifier, position and dimensions
Supports up to 100 persons
Enabled access to object list via CAN and REST interface
Diagnostics & Monitoring
Enabled export of diagnostic file for troubleshooting
Added operational status displaying voltage and temperature
Enhanced, user-friendly warnings and error messages with actionable guidance
Connection Options
Added ethernet configuration to UI
License Mangager
License manger now integrated into application
Improved User Interface
Five new languages available (French, Spain, Korean, Japanese, Chinese)
Introduced new SICK corporate design
Adjusted and improved navigation
Added password strength indicator
3D viewer: Improved layout, legend, coordinate preview, and grid snapping
Bug fixes
Bug fix
Description
FieldConfig API Validation
Points outside valid range are now rejected
CAN Mapping
Corrected mapping for FieldEvaluationResult states (DETECTING_FREE / DETECTING_INFRINGED)
Point Cloud Representation
Fixed incorrect visualization after changing "field of view"-mode
VOI Pixel Display
Resolved issue where pixels disappeared in the volume of interest
UI bugs
Fixed several minor bugs in the user interface
UI links
Fixed broken links to interface description in UI
Known limitations and issues
Limitation or Issue
Description
Unused CAN interface
Activated CAN interface without CAN hardware attached can lead to issues
Video livestream visualization
Video livestream does not show any diagnsotic information
RTSP URL update
After IP address change, the visualized RTSP URL requires a reboot to update
Video livestream distance overlay
Distance of person with bounding boxes at the edge of the screen is not shown
DHCP and RTSP active
Application may crash after restart when DHCP and RTSP are both active
Factory Reset
Requires a second trigger when a non-default password is set
Wrong Link to Interface Description
The UI includes a wrong link to the interface description of the device
IO output mode NPN
Output behaves opposite to expected logic
Factory Reset
Factory reset triggers "access denied" message and requires repetition with default password
Downgrade
After updating to version 2.0.2, it is not possible to downgrade the software to version 1.4.0
Previous releases
Release notes software version 1.4.0 [Click to expand]
New features
Functionality
Description
CAN
Enables a CAN interface based on SAE J1939
2D Live View
Enables a 2D live view via RTSP stream
AI Sensitivity
Advanced filter setting to adjust sensitivity of the AI classification
Ground Plane Filter
Enables filtering of the ground plane for more stable 3D object detection
Improved REST API Functions
Enables additional functions via the REST interface
New AI Neural Network Model
Updated neural network for improved classification of persons
System State Overview
Provides an overview of the current system state and device error logs
Bug fixes
Bug fix
Description
Point Cloud Representation
Fixed a bug that caused incorrect point cloud visualization after switching the field of view mode.
VOI Pixel Display
Fixed a bug that caused pixels to disappear within the volume of interest (VOI).
User Interface
Fixed several minor bugs in the user interface.
Known limitations and issues
Limitation/Issue
Description
DHCP and RTSP Active
The application crashes after device restart when DHCP is enabled and RTSP is active.
Factory Reset
Factory reset does not work when a non-default password is set. In this case, the reset must be triggered a second time.
Field Configuration via API
The API does not return an error when a polygon contains invalid coordinates.
Incorrect Interface Documentation Link
The UI contains an incorrect link to the device interface description.
IO Output Mode (NPN)
The NPN output mode behaves opposite to the expected behavior.
Documentation
Product documentation such as the operating instructions, technical datasheet and mechanical drawings of the Visionary AI-Assist are available on sick.com.
For Software, Software as a Service or Products containing Software, the following terms and conditions shall apply: (i) SICK’s General Terms and Conditions for the Supply of Software Products (“AVB Software SICK”, available at www.sick.com). And/or (ii) SICK’s General Terms and Conditions for Software as a Service (“AVB SaaS SICK”, available at www.sick.com).
This work is protected by copyright. Any rights derived from the copyright shall be reserved for SICK AG. Reproduction of this document or parts of this document is only permissible within the limits of the legal determination of Copyright Law. Any modification, abridgment or translation of this document is prohibited without the express written permission of SICK AG.
The trademarks stated in this document are the property of their respective owner.