web
You’re offline. This is a read only version of the page.
close
Support Portal

CDF600-EtherCAT Technical Information

The technical information for the CDF600-0300 EtherCAT is attached in this article and contains everything you need to know about the CDF600-0300 EtherCAT.
Related Products
CDF600-0300 CONNECT. DEV. FIELDB.
CDF600 EtherCAT

Table of Contents

Introduction

The technical information for the CDF600-0300 EtherCAT can be found in the attachments.
The technical information contains all the informations you need to know about the CDF, e.g.:
  • Functions of the different operating modes
  • Information about electrical connections and cables
  • How to connect different sensor to the CDF
  • How the CDF can be configured
  • Handling on PLC side
  • Data exchange of the CDF
  • Troubleshooting help 

Overview table

Device connected to the CDF Available operating mode Connection method ESI-File
 CLV61x-65x

Proxy-Mode (recommended) 

&

Gateway-Mode 

D-sub device cable to CDF 

ESI-file-CLV61x-F,CLV62x-65x-Proxy 

or

ESI-file-CDF-Gateway

Lector620

Proxy-Mode (recommended) 

&

Gateway-Mode 

17-pin M12 to 15-pin D-Sub cable (6077431)

ESI-file-Lector620-Proxy

or

ESI-file-CDF-Gateway

Lector63x-65x

Lector85x

CLV69x

Gateway-Mode Additional CDB650 or CDM420 required (more details in technical information document)  ESI-file-CDF-Gateway
Lector611 Gateway-Mode

Option 1: use special device cable (2127037)

Option 2: additional CDB650 required (more details in technical information document)

ESI-file-CDF-Gateway

Lector621

RFH6xx

RFU6xx

Gateway-Mode 17-pin M12 to 15-pin D-Sub cable (6077431) ESI-file-CDF-Gateway

IDM Handscanner

Gateway-Mode RS232-Adapter needed (more details in technical information document) ESI-file-CDF-Gateway

Other helpful links

Function blocks for TwinCAT2 and TwinCAT3 can be found here:
CDF600-0300 Downloads

For firmware version see:
Release Notes CDF600-0300

Keywords:
EtherCAT, CDF600 EtherCAT, ESI