accessories
Application
(Show all)What points need to be checked if programming with the PGT-08-S/1036616 does not work?
What points need to be checked if programming with the PGT-08-S/1036616 does not work?
FAQ
(Show all)What SOPAS ET version has to be used for the PGT-08-S?
What SOPAS ET version has to be used for the PGT-08-S?
Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
Are there older SDD files than V2.3 for the PGT-08-S available to program incremental and absolute encoders?
Tutorial
(Show all)How to use the PGT-13-S Emulator Mode (Slave Mode) in combination with a drive
How to analyze a Hiperface DSL encoder with the PGT-13-S Host Mode (Master Mode)