accessories
FAQ
(Show all)How to update the firmware of the PGT-11-S?
Problems with the "Set Position" at the EKS36 / EKM36 (with STM32 controller), in combination with the PGT-11-S
What SOPAS ET version has to be used for the PGT-08-S?
What SOPAS ET version has to be used for the PGT-08-S?
Tutorial
(Show all)How to use the PGT-13-S Emulator Mode (Slave Mode) in combination with a drive
How to analyze a Hiperface DSL encoder with the PGT-13-S Host Mode (Master Mode)
How to use a STSxxx with the PGT-11-S in combination with SOPAS