accessories
Application
(Show all)How can the two error outputs for fan and temperature monitoring be checked on the TPCC cooling housing?
Description
Why is the cooling element of the TPCC cooling housing not activated during commissioning despite the high ambient temperature?
Description
Steel industrie - Detection of steel slabs ( > 600°C)
Application to detect hot metallic objects used in the steel industry.
FAQ
(Show all)Where is the position of the optical axis of a sensor mounted inside TPCC cooling housing?
This article describes how to find the position of the optical axis of a sensor mounted inside TPCC cooling housing.
How to mount a distance sensor inside the optional TPCC cooling housing from accessory
This article describes how to mount a distance sensor inside the optional TPCC peltier cooling housing from accessory