detection sensors
Application
Inductive Sensors for flushed mounting used non-flush
Inductive Sensors for flushed mounting used non-flush > reduced scanning range
Battery foils double layer detection with IMC12 or IMC08
The article recommends to use IMC12 or IMC08 (idf-inductive double foil version) to detect double layers, for example in battery foils.
Tooth Detection on Toothed Wheel or Fanblade on Fanwheel
Tooth detection on toothed wheel or fanblade on fanwheel
Presence Detection of RFID-tags on the Carrier Foil
Presence Detection of RFID-tags on the Carrier Foil with inductive sensor.