motion control sensors
Application
(Show all)What points need to be checked if programming with the PGT-08-S/1036616 does not work?
Mounting Rotary Encoders- Guidelines, Information & Mounting Videos
FAQ
(Show all)Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
What screws are usually used to mount the stator coupling to the hollow shaft encoders?
Tutorial
(Show all)How a tiltrotator application can be solved via AHM36 CANopen
This tutorial shows how to configure a AHMx36 to event-timer (time based communication) via PCAN-View.