motion control sensors
linear encoders - Latest Knowledge Articles
Application
(Show all)How to mount an encoder with face mount flange onto an EG34x safety limit switch?
How to mount an encoder with face mount flange onto an EG34x safety limit switch?
FAQ
(Show all)What does it have to do with the universal electrical interface "F" of the DBS60?
How to mount the wire guide pulley to the MRA-F080?
How are the switching contacts of the EG34x arranged?
Tutorial
(Show all)The ETL70 (Hiperface DSL) in combination with the PGT-13-S
The STL70 (Hiperface) in combination with the PGT-11
How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?
How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?