motion control sensors
Application
(Show all)What points need to be checked if programming with the PGT-08-S/1036616 does not work?
Mounting Rotary Encoders- Guidelines, Information & Mounting Videos
How to mount an encoder with face mount flange onto an EG34x safety limit switch?
FAQ
(Show all)Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
What screws are usually used to mount the stator coupling to the hollow shaft encoders?
Tutorial
(Show all)How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?