motion control sensors
FAQ
(Show all)Is it possible, to cut the magnetic tape of a TTK70, TTK50, STL70, ETL70 into pieces and use the single pieces as measuring track?
additional information to the magnetic linear encoder L230 with Hiperface or SSI
What electrical interface is set by default for programmable incremental encoders?
Tutorial
(Show all)How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?