motion control sensors
FAQ
(Show all)The L230 (LinCoder) linear encoder
additional information to the magnetic linear encoder L230 with Hiperface or SSI
What electrical interface is set by default for programmable incremental encoders?
What electrical interface is set by default for programmable incremental encoders?
Are the mounting kits to mount the encoders to the HighLine wire draw encoders available as a spare part?
Are the mounting kits to mount the encoders to the HighLine wire draw encoders available as a spare part?
Tutorial
(Show all)How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?
How to convert the SSI interface of an encoder into the parallel interface with the converter box IP210 from Motrona?