detection sensors
Application
(Show all)Side detection of a beam splitter
The article explains how to detect a certain side of a beam splitter.
How to detect ultra small holes with fibers
This article shows how to configure an fiber amplifier to detect ultra small holes in a circuit board using SopasET.
Mixing WLL80 and WLL180T in a gang mount setup
Description
FAQ
(Show all)Is it possible to use two fiber amplifier with the same fiber as sender-receiver combination?
Description
Can all types of fiber optic cables be used in potential explosive atmospheres?
Description
Is it possible to use all outputs of the connected amplifiers with the Smart Task function of the WI180C-IOA00?
Description