detection sensors
Application
(Show all)PCB detection with fibers
This article provides an example of printed circuit board detection using through beam optical fibers and amplifiers.
WLL80 Anti Interference in bus
Side detection of a beam splitter
The article explains how to detect a certain side of a beam splitter.
FAQ
(Show all)Is it possible to use two fiber amplifier with the same fiber as sender-receiver combination?
Can all types of fiber optic cables be used in potential explosive atmospheres?
Is it possible to use all outputs of the connected amplifiers with the Smart Task function of the WI180C-IOA00?