detection sensors
Application
(Show all)Optical synchronization simplifies installation and reduces wiring complexity. Maintaining one clear SYNC beam is critical for full functionality.
How to interpret the quality of process score for the MLG-2 Pro
FAQ
(Show all)GSDML files define PROFINET devices for engineering tools, including identity, interfaces, module structure, and version details.
Configured settings reset after PLC restart if a configuration module/assembly is active. Remove it or adjust parameters to prevent overwrites.
how to connect 2 x MLG2-Pro RS485 to one RS485 Communication Modul and how to configure the MLG's