web
You’re offline. This is a read only version of the page.
close
Support Portal

Are there older SDD files than V2.3 for the PGT-08-S available to program incremental and absolute encoders?

Table of Contents

Yes, there are still older SDD file versions than V2.3 for the PGT-08-S available.

 

Those old SDD files are necessary if e. g. a customer has made an old backup file from an old encoder that he has programmed with the PGT-08-S or the customer has an programmable encoder with an older firmware version.

 

In the following table you get an overview of the different and available SDD file versions and the date of their publication.

 

 

SDD file version date of publication Name of file
V1.0 02/20/2013 PGT08S_v1.0.sdd
V1.1 06/29/2015 PGT08S_v1.1.sdd
V2.0 07/31/2015 PGT08S_v2.0.sdd
V2.1 09/20/2016 PGT08S_v2.1.sdd
V2.3 03/02/2023 PGT08S_v2.3.sdd
V2.2 latest version PGT08S_v2.2.sdd

You will find the different SDD file versions to download in the attachment.

Keywords:
SDD files, PGT-08-S, programmable encoders, incremental, abolute, V1.0, V1.1, V2.0, V2.1, V2.3