LiDAR and radar sensors
FAQ
In the operating instructions we state the following:- typically 4 x 3 mm (viewing window)- 2.5 x 2mm (3m distance)
The laser diode of the LMS4000 emits light radiation at 660nm. The filter bandwidth of the LMS4000 receiving unit is +/- 30nm.
The sensor works with 2 frequencies: 120 MHz and 99 MHz. The unambiguous range is about 7.14 m
The sensor uses a focusing lens and aperture, so the "classic" case, i.e., a certain size at the window and defined divergence, does not exist. The point o