LiDAR and radar sensors
Application
(Show all)This article provides additional information and instructions to the CoLa A and CoLa B protocol as well as the corresponding software modules and examples.
Remission values of various surfaces
This table helps to compare the CoLa AB telegrams across all device families.
FAQ
(Show all)This page explains how to find the device IP address without SICKs discovery function.
You can create a 3D point cloud using Sopas ET with LMS4000. In this article, there are some hints to this function.
In the operating instructions we state the following:- typically 4 x 3 mm (viewing window)- 2.5 x 2mm (3m distance)
Tutorial
(Show all)Describes an example of what the LMS4000 is capable of performing automated tasks.
Description
The macros enable you to play around with published telegrams for the LMS4000.