LiDAR and radar sensors
Application
Description
This article provides additional information and instructions to the CoLa A and CoLa B protocol as well as the corresponding software modules and examples.
Remission values of various surfaces
This table helps to compare the CoLa AB telegrams across all device families.
This article contains several ROS 2 bag files with topics of the multiScan136, multiScan165, picoScan150 and an IP camera. The data were captured using a C
How-To Videos of multiScan
This article provides additional information and instructions to the REST API communication interface as well as the corresponding software modules and exa
This article provides additional information and instructions to the Compact and MSGPACK data format as well as the corresponding software modules and exam
Entry point for LiDAR ROS Driver
This article contains several rosbags recorded with ros2. The scene has been captured in a vine with multiScan136/165 + IP camera
Description
Description
Tutorial to change parameter via the REST API