web
You’re offline. This is a read only version of the page.
close
Support Portal
Public mode with limited access to support knowledge articles. For full functionality, please log in or register. Details about the registration process can be found here.

picoScan100 - Latest Knowledge Articles

View in product catalog
Application
picoScan100: FDA Accession Number

This page contains information about the picoScan100 FDA accession number.

picoScan150: Possible challenges and countermeasures in outdoor applications

This page considers outdoor conditions and lists the corresponding specifications and integrated measures. Then, possible additional measures are explained

picoScan100: How-to videos?

This extensive collection of picoScan100 video tutorials is designed for users of all levels, from beginners to advanced.

picoScan100: RSSI Scaling

This page provides information about the RSSI scaling with different output formats.

2D LiDAR Mutual Interferences (HDDM+)

This page explains how 2D LiDARs overcome mutual interferences with HDDM+.

Protocol and Integration: CoLa

This article provides additional information and instructions to the CoLa A and CoLa B protocol as well as the corresponding software modules and examples.

Typical remission values of different materials

Remission values of various surfaces

CoLa A/B Device Compatibility Table

This table helps to compare the CoLa AB telegrams across all device families.

picoScan100: How to get the device status information?

The picoScan100 has several options for providing information about the device's availability. These features are described in the following article.

picoScan100: How to improve the measurement performance in stationary applications?

The measurement performance of the picoScan can be optimized for different targets. If the material to be measured is known, various actions can improve th

multiScan100/picoScan100: rosbag recordings - corn chopper

This article contains several ROS 2 bag files with topics of the multiScan136, multiScan165, picoScan150 and an IP camera. The data were captured using a C

Protocol and Integration: REST API

This article provides additional information and instructions to the REST API communication interface as well as the corresponding software modules and exa

Protocol and Integration: Compact & MSGPACK

This article provides additional information and instructions to the Compact and MSGPACK data format as well as the corresponding software modules and exam

picoScan100: native ROS2 (Linux/Windows)

This tutorial explains how to run native ROS 2 on a picoScan150 within a ROS 2 environment.

How to install the Insomnia plugin to fix “Access Denied” during HTTP POST request?

Tutorial to change parameter via the REST API

picoScan100: rosbag recordings

picoScan100 data recordings in rosbag format.