web
You’re offline. This is a read only version of the page.
close
Support Portal
Public mode with limited access to support knowledge articles. For full functionality, please log in or register. Details about the registration process can be found here.

linear encoders

FAQ
What does it have to do with the universal electrical interface "F" of the DBS60?

Description

How to mount the wire guide pulley to the MRA-F080?

Description

Is it possible to use the wire pulley for all HighLine mechanics?

Description

What material is the flange of the AFS60 / AFM60 Inox made out of?

Description

What material is the housing of the AFS60 AFM60 Inox made out of?

Description

What kind of stainless steel is used for the DBS60I?

Description

What kind of screws are needed to install the optional tether on the DGS35?

Description

Is is possible to mount an encoder on both sides of the VarioLine wire draw mechanic?

Description

How to mount the wire guide pulley to the MRA-F130?

Description

What sizes of encoders can be mounted on the VarioLine wire draw mechanics?

Description

The L230 (LinCoder) linear encoder

additional information to the magnetic linear encoder L230 with Hiperface or SSI

What electrical interface is set by default for programmable incremental encoders?

What electrical interface is set by default for programmable incremental encoders?

Are the mounting kits to mount the encoders to the HighLine wire draw encoders available as a spare part?

Are the mounting kits to mount the encoders to the HighLine wire draw encoders available as a spare part?

What are the dimensions of the cable from the ACx36/ACM60?

What are the dimensions of the cable from the ACx36/ACM60?

What type of groove spring is used for the ACx36?

What type of groove spring is used for the ACx36?

How long is the A3M60A-S4P with the mounted connectors of the cables?

Description

How to replace a DGS65 with a DFS60?

How to replace a DGS65 with a DFS60?

What is the task of a pulley/deflection roller when using with a wire draw encoder?

What is the task of a pulley/deflection roller when using with a wire draw encoder?

Troubleshooting when programming the ACx36/ACM60

Troubleshooting when programming the ACx36/ACM60

Can an encoder be mounted on the other side of the wire draw mechanism?

Can an encoder be mounted on the other side of the wire draw mechanism?

Are there spare parts for the wire draw mechanisms available?

Are there spare parts for the wire draw mechanisms available?

What default output settings do the ACx36/ACM60 encoder have?

What default output settings do the ACx36/ACM60 encoder have?

How can I mount the encoder with clamping/face mount flange on the MRA?

How can I mount the encoder with clamping/face mount flange on the MRA?

Is it possible to change the electrical interface of the DUS60?

Is it possible to change the electrical interface of the DUS60?

What happens if you do a RESET at a wire draw encoder with analogue output?

What happens if you do a RESET at a wire draw encoder with analogue output?

What is maximum tightening torque of the screws to install the optional stator coupling on the DGS35?

What is maximum tightening torque of the screws to install the optional stator coupling on the DGS35?

What is needed to mount the DGS3x with the pin-block?

What is needed to mount the DGS3x with the pin-block?

What kind of screw is used for the clamp ring of DGS35?

What kind of screw is used for the clamp ring of DGS35?

What values are valid for the current output of ACx36/ACM60?

What values are valid for the current output of ACx36/ACM60?

What is the maximum tightening torque for the clamp ring screw of DGS35?

What is the maximum tightening torque for the clamp ring screw of DGS35?

Are there accessories for the VarioLine wire draw encoder available?

Are there accessories for the VarioLine wire draw encoder available?

Is there a functionblock for the IO-Link devices available?

Is there a functionblock for the IO-Link devices available?

What to do if you have a DFS60 with expanding shaft?

What to do if you have a DFS60 with expanding shaft?

What does it mean if a DFS60 has a number as hollow shaft size (e.g. DFS60x-T5xx...)?

What does it mean if a DFS60 has a number as hollow shaft size (e.g. DFS60x-T5xx...)?

What is it about if a DGS6x has the letter E, K, L or N as electrical interface?

What is it about if a DGS6x has the letter E, K, L or N as electrical interface?

Is there a tool for loosening and tightening M12 plug connectors available?

Is there a tool for loosening and tightening M12 plug connectors available?

How to replace a DRS60/61-xAxxxxxx or DRS60/61-xDxxxxxx?

How to replace a DRS60/61-xAxxxxxx or DRS60/61-xDxxxxxx?

Is there a multiturn encoder available with parallel output?

Is there a multiturn encoder available with parallel output?