web
You’re offline. This is a read only version of the page.
close
Support Portal
Search our Knowledge Base for instant answers or create a request to connect directly with your local SICK expert for quick resolution. For full functionality simply log in in with your SICK ID or register.

incremental encoders

FAQ
What screws are usually used to mount the stator coupling to the hollow shaft encoders?

What screws are usually used to mount the stator coupling to the hollow shaft encoders?

Which servo clamps can be used for which encoder? In which pitch circle diameter do the servo clamps have to be mounted?

Description

What encoder groups are there for encoders with a servo flange regarding the centering and the servo groove width/diameter?

Description

Is there a signal distributor for encoders with TTL/HTL interface available?

Is there a signal distributor for encoders with TTL/HTL interface available?

What is the difference between static and dynamic shaft movement at encoders and motor feedback systems

Description

Are there older SDD files than V2.3 for the PGT-08-S available to program incremental and absolute encoders?

Description

What is the recommended tolerance that the drive shaft should has to mount the hollow shaft encoders?

Description

Is there an overview for the minimum drive shaft length for all through hollow shaft encoders?

Description

Is there an overview for the minimum and maximum drive shaft length for all blind hollow shaft encoders?

Description

What does it have to do with the universal electrical interface "F" of the DBS60?

Description

What screws and washers are needed to mount the standard stator couplings of the hollow shaft encoders?

Description

What rotary encoders are available with a blind hollow shaft and with what shaft diameters?

Description

How to mount rotary encoders with a blind or through hollow shaft?

Description

How to mount rotary encoders with a square flange?

Description

What screws are needed to mount solid shaft encoders with a square flange?

Description

What solid shaft encoders are available with a square flange and what characteristics do they have?

Description

What screws are needed to mount solid shaft encoders with a servo-/face mount flange?

Description

What servo clamps can be used for rotary encoders with a servo-/face mount flange? In which pitch circle diameter do the servo clamps have to be mounted?

Description

What solid shaft encoders are available with a servo-/face mount flange and what characteristics do they have?

Description

How to mount rotary encoders with a face mount flange using the mounting spigot?

Description

How to mount rotary encoders with a face mount flange using own mounting brackets?

Description

How to mount rotary encoders with a face mount flange using mounting brackets?

Description

What is the mounting spigot and how does it work?

Description

What screws are needed to mount solid shaft encoders with a face mount flange?

Description

Which mounting bracket can be used for which encoder?

Description

What encoder groups are there for encoders with a face mount flange regarding the centering?

Description

What solid shaft encoders are available with a face mount flange and what characteristics do they have?

Description

What is the maximum length that the shaft stub can be if the mounting bell is fixed directly to the application?

Description

What problems might arise with the mounting bell in relation to the coupling?

Description

How to mount rotary encoders with a servo flange using the threaded holes of the encoder with & without a centering?

Description

How to mount rotary encoders with a servo flange using the half shells?

Description

How to mount rotary encoders with a servo flange using the mounting bell?

Description

How to mount rotary encoders with a servo flange using the servo clamps?

Description

What screws are needed to mount solid shaft encoders with a servo flange?

Description

What solid shaft encoders are available with a servo flange and what characteristics do they have?

Description

What activities must be reviewed before and after the mounting of rotary encoders?

Description

What tools and aids are needed to mount rotary encoders?

Description

What safety guidelines must be strictly followed for mounting rotary encoders?

Description

What is distinctive for a rotary encoder with a blind hollow shaft?

Description

What is distinctive for a rotary encoder with a through hollow shaft?

Description

What is distinctive for a rotary encoder with a square flange?

Description

What is distinctive for a rotary encoder with a servo-/face mount flange?

Description

What is distinctive for a rotary encoder with a face mount flange?

Description

What is distinctive for a rotary encoder with a servo flange?

Description

What mechanical interfaces are available with the rotary encoders?

Description

What kind of stainless steel is used for the DBS60I?

Description

Are all programmable DFS2x encoders programmable?

Description

Is the metal shaft collet with a diameter of 1/4" for the DUS60 also available as a spare part and in plastic?

Is the metal shaft collet with a diameter of 1/4" for the DUS60 also available as a spare part and in plastic?

What resolutions are possible with the DGS80?

What resolutions are possible with the DGS80?

What electrical interface is set by default for programmable incremental encoders?

What electrical interface is set by default for programmable incremental encoders?

How to replace a DGS65 with a DFS60?

How to replace a DGS65 with a DFS60?

Is it possible to change the electrical interface of the DUS60?

Is it possible to change the electrical interface of the DUS60?

What to do if you have a DFS60 with expanding shaft?

What to do if you have a DFS60 with expanding shaft?

What does it mean if a DFS60 has a number as hollow shaft size (e.g. DFS60x-T5xx...)?

What does it mean if a DFS60 has a number as hollow shaft size (e.g. DFS60x-T5xx...)?

Is the clamping ring for the hollow shaft encoders as a spart part available?

Is the clamping ring for the hollow shaft encoders as a spart part available?

How to replace a DG60 with a 6x19mm solid shaft recognizable by the third typecode letter "B"?

How to replace a DG60 with a 6x19mm solid shaft recognizable by the third typecode letter "B"?

What incremental encoder has the lowest standard start up and operating torque?

What incremental encoder has the lowest standard start up and operating torque?

Is there an encoder available with an higher operating speed than 9000 rpm?

Is there an encoder available with an higher operating speed than 9000 rpm?

What is it about if a DGS6x has the letter E, K, L or N as electrical interface?

What is it about if a DGS6x has the letter E, K, L or N as electrical interface?

Has the design of the clamping ring for the hollow shaft encoders been changed?

Has the design of the clamping ring for the hollow shaft encoders been changed?

What is the tolerance of the tightening torque from the clamping ring screw of hollow shaft encoders?

Description